Hello
I have been trying to design a 12V to 5V 5A switching regulator and I have used TI's TPS565208 to perform this. I have followed the designed guideline on the datasheet. I do get 5V output when there is 12V at the input but output goes to zero when I connect any load across the 5V output. I measured pin 2 (SW) there is no switching happening. The load I'm connecting is 1K across the 5V (I have also tried putting 10R). I measured the inductor current and again no switching ripple. I doubt it is switching at all and outputting something arbitrary. Enable pin EN has been pulled to high.
This ideally should be pretty straight forward design - don't understand why the IC does not start up. Can you help?
regards
Nilanjan