Hi all,
I enable the IR compensation by setting REG08[4:2] to 0x1 and REN08[7:5] to 0x1.
The expected battery CV voltage should be VREG_actual = VREG (4.208V) + min (Ichrg_actual(1800mA) x BATCOMP(20mohm), Vclamp(32mV))
However I observed the battery CV voltage was still same as VREG (4.208V).
Is any thing I missed to config other register? Or what should I do to debug that ?
Thanks.