Hi,
I have a question regarding bq7693000+bq78350-r1 application: can the cell balancers be on and running as close as possible to 100% duty cycle whenever cell voltages are above 3.65 V? If it can, how should I configure the cell balancing related parameters in gg file? Please advise.
By the way, in the application, the charger will be always connected with the BMS.
Thanks,
Joy