Part Number: LM5116
Hi Tiers:
I use the LM5116 in my DC/DC project
input:50V
ouput:12V1A
when the load is CC<0.6A, all waveforms are normal.
but when the load is CC>0.6A, the waveform is not normal, just as below:
C2 is low-side MOS gate driver
C3 is the Inductive current waveform
All the SCH parameters are from the Webench.
Could you give me some suggestions to deal with this issue? thx