Other Parts Discussed in Thread: TPS61099
Hi,
I was wondering is there a way to set the default DC/DC output to 3.0V... This family of parts has everything I need except I need it to run it @ 3.0V upon power up
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I was hoping to use the SYS output as the main rail for my device... My MCU is NFS52310, though it can run at 1.8V, I have a few other devices running at the 3.0V (RGB led and driver)... Do you think the LDO can drive the RGB led (Wurth Part #150044M155260) and driver (Kinetic Part #KTD 2026) which by rough calculations should be under 100mA
The LDO should be fine as long as the load is below 100mA. You can power the MCU from the DCDC and adjust the LDO voltage after startup.