Hi
1. Output voltage is 12.23v when DC input is 11-13v;
- VDD =VREG =6V
- CELL_BATPRESZ =3.8V;
- ILIM_HIZ = 2.8V;
2. When adjusting the input of 5~11V, the input current keeps jumping and cannot be stabilized.
And the sound of "drip drip drip drip";
3. Adjust CELL_BATPRESZ voltage divider, the output does not change;
Please suggest how to troubleshoot.
Thanks
Star