Hello,
What is the average current consumption of the TPS63031 when the EN pin goes high? Is it higher than the RP604K331A by Ricoh Electronics?
Thank you,
Kyle Wisbrock
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
What is the average current consumption of the TPS63031 when the EN pin goes high? Is it higher than the RP604K331A by Ricoh Electronics?
Thank you,
Kyle Wisbrock
Hi Kyle,
I assume you are referring to the no-load input current. This depends on mode of operation. For the explanation of power modes refer to section 7.4.4 of the TPS63020 datasheet, the principle is the same in the TPS63031:
RP604 has significantly lower Iq, so I assume the no-load input current is below 1 μA, but this should be verified on the real circuit.
PS. To understand what Iq is and how to translate this to the real current consumption, check this application note:
IQ: What it is, what it isn’t, and how to use it
Best regards,
Milos
Hi Kyle,
We haven’t heard back so we're assuming this resolves your issue. If not, just post a reply below, or create a new thread if the thread has locked due to time-out.
Thanks and regards,
Milos