This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24703: BQ24073RGTR Not charging battery

Part Number: BQ24703
Other Parts Discussed in Thread: BQ24073

Dear Support,

I have designed a PM circuit to charge a battery using the BQ24073RGTR.  Here is what it is doing:

- I connect USB... 5V go in, and 4.4V come out at Pins 11, and 10.

- Both EN1, and EN2 are low to indicate 100mA draw from the USB.  Please not that USB bus is not yet enumerated to draw 500mA so I am assuming 100mA max

-TD Pin15 is made low (enabled) via 10K external pull-down resistor so charge disabled is not constantly charging the battery

- CE_N is low via 10K pull-down resistor to enable charging with low current max 100mA (system load requires 3mA, 97mA for battery)

-EN1 and EN2 are pull-down externally via 100K resistors pull-downs

- TS PIN 1 was changed from 49.9K to 10k pull-down since there is no thermistor.

- ILIM is set to 1.18K external resistor

-ISET is set to 5.90K assumes 750mAH battery with 0.2C charging (150mA)

-TMR is set to 47K resistor.

I see the voltage come out, I see PGOOD_N going low and enabling a green LED... I see CHG_N (pin9) going low indicating it is charging, but it is not... when I put an DMM in current mode to measure the charging current into the battery, it reads 0A.  No current is being delivered into the battery.  I don't understand what could be wrong if all parameters appear to be in order.

Any idea as to why the charger would not charge the battery?

  • Hi Roberto,

    Based on the pin names you mentioned, it sounds like you're using the BQ24073, not the BQ24703. Is this correct?

    If so, can you please create a new thread with the BQ24073 in the title? Please also share your schematic.

    Best regards,

    Angelo