This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28019A: UCC28019A Audio noise issue

Part Number: UCC28019A


My client tested the UCC28019A to be noisy at no load.

Test conditions are as follows:

VAC 220VAC/ no load.

After measuring the prototype I found to have audio noise, the VCOMP voltage is 1.4V lower than the normal (no audio noise) prototype.( normal  VCOMP :1.5~1.9V),

I have added 1.5M ohm between VCC and ICOMP, which can solve the test problem. I have tried to adjust the ICOMP and VCOMP parameters and can't solve it. Is there any way to eliminate the noise of the UCC28019A by adding 1.5Mohm?