This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61022: TPS61022 Feedforward Capacitor Selection

Part Number: TPS61022

Hello,
I have developed a power supply for a GSM module but have problems with loop stability.
The datasheet says:
For large output capacitance more than 40 μF application, TI recommends a feedforward capacitor to set the zero frequency (fFFZ) to 2 kHz.
What is meant by zero frequency in this case? Is this the right plane zero frequency without feedforward capacitor? Does it depend on the load transients or on the switching frequency of the boost?

Best regards
Raphael