This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3839: Higher Temperature range variants?

Expert 6460 points
Part Number: TPS3839
Other Parts Discussed in Thread: TPS3840, TLV803E

Team,

are there plans to have TPS3839G25DBZR in wider T range variants? (current device is up to 85C ambient).

Thanks.

  • Hi Bart,

    There are no current plans to extend temperature range currently, but I recommend taking a look at the TPS3840. This device also has nano-Iq and it is a recent release with improvements for our devices.

    If 3 pin simplicity is required without /MR, consider looking into the TLV803E.

    Both of these devices support up to 125 C.

    Thanks,

    Abhinav.