This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS562200: Is SW node in high impedance mode when input power is off ?

Part Number: TPS562200

Hi, 

I am considering using TPS562200 to convert 12v to 5v supply.

In some cases, 12V power may be removed and I still need to keep 5v output up by connecting it to other power rail.

Just wonder whether that is a 4iwk since current may flow through the inductor without control if SW node is pulled to ground instead of high-z?

Thanks