This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28703: I am after a 20mA PWM constant current regulator

Part Number: UCC28703


Hello,

I am after a 20mA constant current PWM regulator for an audio class G/H power stage, see the attached schematic to replace linear transistor Q1 & Q2.

Must work from 2 Volts to 300 Volts.

What part do I need?

4000W amp Power Stages.pdf