This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27542-G1: BQSTUDIO not detect ic- bq27542

Part Number: BQ27542-G1
Other Parts Discussed in Thread: BQSTUDIO, EV2400

i installed bqstudio on windows 10. my i.mx6 board connected with bq27542. but bqstudio unable to detect this ic. what i have to do to connect bqstudio with bq27542.

1. howmany ways to connect it? and which is easy way to do it? is any extra hardware require to do it? if yes then tell that hardware name ?

2. if any stepwise guide is there then please give information about it(quick start guide).

3. is it possible to run bqstudio on linux. if possible then give steps to install it.

4. i try to get remaining battery charge in percentage which is increasing  run time while charge it till full charge and decreasing runtime while it dishcharge.

4.1] i use driver bq27xxx i2c.c but i want to get just charge percentage which steps i have to follow to get it.

4.2] without gauging configuration is it possible to get exact charge percentage? if not then which things i have to take care while implement code?