I have an issue where the BQ24725AEVM-710 is not passing current from the supply to the load.
I first set the evaluation kit up according to Figure 2 in the User Guide and fail to get the correct voltages at the test points.
ACDRV and CMSRC read as 0.
J2 also does not have the correct values.
When I hook up a load to J2(Bat, GND) no current passed to the load
When I hook up a load to J2(SYS, GND) no current is passed to the load
When I hook up a load to J2(SYS, GND) and J2(BAT, GND) no current is passed to either load.
I was hoping that someone could help identify the problem and / or point me at least in the right direction.