Other Parts Discussed in Thread: LMR16030, LMR16020, LMR16010
LMR14020 This chip I want to use as BUCK-BOOST topology, output negative voltage, input +18 to 30V output negative 24V, so need a relatively large duty cycle range, up to 0.6 or so, the specification says that when the switching frequency is 200kHz I can get the maximum duty cycle. I want to know the maximum duty cycle that this chip can provide at the highest switching frequency. Because I want to reduce the inductance, I want to use a chip with a higher switching frequency. Which more suitable models are recommended for me? Please give me some advice, thank you very much!