This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78PL116: Aux Chem File Utility crash

Part Number: BQ78PL116

In the past, I've make several *.aux files. But with a new 7S8P 24Ah pack, it's seem impossible.

I make the cycling sequence : 12A discharge, 12A on/off charging, 16,8A charge, then 12A finale discharge.

Issue :

The Aux Chem File Utility crashes ...

- I've already make an aux file with a 19Ah pack. 

- With a bigger pack, and a IPscale = 10, current in the csv are divided, and aux file is generated.

If I divide by 10 all current (I) values in the CSV, it works!

Is there a current limit in the Aux Chem File Utility ? 

Nicolas