This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25982: Max Cout value of TPS259827

Part Number: TPS25982

Hi

My customer use TPS259827 under Vin=24V and Cout=1200uF.
But it don't operate. I think that the thermal shutdown operat because of  too big Cout.
What is the max value of Cout being able to use under Vin=24V? 

Best regards,
Yokota