Other Parts Discussed in Thread: BQ25890
Hello,community
I asked the following questions and got answers.
Regarding “it will allow current to flow from BAT to SYS in supplement mode as needed”, what is the state when the FET turns on in supplement mode?
question
(1)When charging is complete, turn off the battery FET.
At this time, when the VSYS (REG) voltage rose to VBATREG + 3%, it was read from the data sheet.
Maintain the Not high impedance mode with the IN or USB input connected.
Load from SYS pin.
Since the FET is off, is it supplied to the SYS pin load from the IN or USB input?
anser
Regarding 1, even if battery charging has terminated and the BATFET doesn't allow current to flow from SYS to BAT, it will allow current to flow from BAT to SYS in supplement mode as needed.
Best Regards,
Goto