This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL1431-SP: package dimensions & material

Part Number: TL1431-SP

Could you let me know the package information as follows?

P/N:
5962-9962001VPA

・Package material/ base plating /plating (ex. Ceramic(Alumina)/Ni/Au

・Lid material/ base plating /plating (ex. Covar/Ni/Au

・Package cavity wall thickness(mm) (ex. 0.25mm

・Lid thickness(mm) (ex. 0.25mm

・Part weight(typ. grams) (ex. 3.5g

・Part weight(max. grams) (ex. 4.0g


We'd like to use it for a thermal & radiation analysis.


Regards,
Tomcavity wall and lid definition.pdf