This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2660: SHDN Pin Of TPS26601 ; No.2

Part Number: TPS2660

Hi,

I ask you a question by addition because there is not the answer that I need about this pin.

If I make pulling up external, how much of voltage and impedance  should I do pulling up?
Can I make pulling up with the Vin(max. 55V) voltage?

Regards,
PAN-M