This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD87330Q3D: Recommended part for higher ESD(HBM) rating

Part Number: CSD87330Q3D
Other Parts Discussed in Thread: CSD87335Q3D, CSD87333Q3D, CSD87334Q3D, CSD86330Q3D, CSD86336Q3D, CSD87331Q3D, CSD17302Q5A

Hi Team,

My customer is using CSD87330Q3D but its ESD rating is only 200V. Do we have P2P or similar solutions that has 500V HBM rating to be promoted to customer?

Thanks a lot.

Vincent Chen

  • Hi Vincent,

    Thanks for promoting TI FETs at your customer. Below is a list of all parts in the Q3D (3.3 x 3.3mm SON) package and the HBM pass voltage. The CSD87333Q3D and CSD87334Q3D include ESD protection diodes and have a much higher HBM pass voltage. However, these devices are optimized for high duty cycle operation and have symmetric FETs (same size die and rds(on) ratings). The only other power block in this package that come close is the CSD87335Q3D which passes 400V HBM.

    CSD86330Q3D 250V
    CSD86336Q3D 300V
    CSD87330Q3D 200V
    CSD87331Q3D 150V
    CSD87333Q3D 3000V
    CSD87334Q3D 4000V
    CSD87335Q3D 400V
  • Hi John,

    Thanks very much for you comment.

    My customer is asking for ESD rating of CSD17302Q5A, could you please also help on this case.

    Best regards,

    Vincent Chen

  • Hi Vincent,

    The CSD17302Q5A passes 250V HBM and 2000V CDM.

  • Hi John,

    Got it, thanks very much for prompt response.

    Best Regards,

    Vincent Chen