Hi,team.
Is there a possibility that the #FLT pin of TPS16630RGET will output an L signal when the power is turned on?
In our circuit, the #FLT pin is connected to the CPU and pulled up.
When the CPU detects the L signal, it performs error processing.
Since the CPU starts up first and powers on the TPS16630RGET, if the TPS16630RGET outputs an L signal for a moment during startup, it will be recognized as an error.
thanks.