This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Buck Converter

Other Parts Discussed in Thread: TPS54531, BQ500101, LM73605

Hi, I need to make buck power stage for 30W heater working witch 24V input voltage,  and working temperature about 100 degree. I thought about use BQ500101, but this IC has no thermal protection. So my next idea was to use voltage buck regulator such as TPS54531 and use EN or FB pin for control output voltage. Could you tell me if that sollution may works good? Maybe other better solution? The gool is to maximum simplisity of power stage and current and thermal protection.