This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/UCC256302: Key parameter for FET selection

Part Number: UCC256302

Tool/software: WEBENCH® Design Tools

Hello experts,

I have question for FET selection of power design which use UCC256302.

In datasheet 7.2.2.13, there is description "The slew detection circuit has a detection range of 1V/ns to 50 V/ns."

For this detection range, what electrical characteristic of FET should I take care?

Thanks and best regards,

Ryo Akshi