The maximum fluctuation range of DAPWM is 0.05. Assuming that the sampling high voltage is 600V,
Suppose that the upper sampling resistance of the inlet AD port is 800k and the lower sampling resistance is 3.3k.
the actual value of AIN at the inlet of AD port is 2.46v,It's about 2.5 volts ,
In normal state, APWM output duty cycle is 0.5, but APWM output duty cycle may fluctuate to 0.55
then in the software
the value of AIN at the inlet of AD port is 2.25v.
Multiplied by the magnification factor, 0.25*(800+3.3)/3.3=60.856V ,the sampling voltage accuracy is sixty volts, am I wrong?