Other Parts Discussed in Thread: LM5069
Hi
My customer uses PSU with LM5069EVM-627, the second startup will abnormal, as below
What could be the reason?
There are currently actions is off UVLO, increst timer capacitor, add D2, R6..etc
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
My customer uses PSU with LM5069EVM-627, the second startup will abnormal, as below
What could be the reason?
There are currently actions is off UVLO, increst timer capacitor, add D2, R6..etc
Hi Bryan,
What is the load at the output of LM5069EVM-627 ?
Can you send me a test waveform including current information as well. Please include a image files for better readability.
In the test waveform please include
Thanks
Rakesh
Hi Bryan,
Thank you. What is the source ? Is it from PSU.
Are you seeing the similar behavior when tested from DC power supply.
BR, Rakesh
Hi Bryan,
Thank you.
Please do following two tests by making below changes on EVM.
Test-1: Leave jumper JMP1 OPEN
Test-2: Configure the EVM as per Figure 4. Re-design the values of R1, R2, R3 and R4 to set UVLO at 23V and OVLO at 28V
Also send me zoom-out waveform (above waveforms) in 1ms/div to see the behavior at the first instant
BR, Rakesh
Hi Rakesh:
No, I didn't.
Recently customer add discharge circuit in EVM input,
speed up the discharge at the input
It can improve this situation, input and output voltage can rise up smooth.
Just curious why not discharge completely has this behavior.
Hi Bryan,
When the input voltage drops near to UVLO threshold, LM5069 switches off the path and hence the input voltage stays there if there is no discharge path.
BR, Rakesh
Hi Rakesh:
Current set up of way, indeed input drop to UVLO, the input voltage will stay there,
when the next turn on input, it should rise up smooth, actually not unstable,
Is it possible that the range of hysteresis is not enough?
UVLO keep EVM set : Lower UVLO threshold is 17V
Upper UVLO threshold is 18V
Hi Bryan,
May be.. that's the reason I asked to check by shifting the UVLO thresholds
Please do following two tests by making below changes on EVM.
Test-1: Leave jumper JMP1 OPEN
Test-2: Configure the EVM as per Figure 4. Re-design the values of R1, R2, R3 and R4 to set UVLO at 23V and OVLO at 28V
Also send me zoom-out waveform (above waveforms) in 1ms/div to see the behavior at the first instant
BR, Rakesh