Hi,
PIN IN&P_IN is supplied independently. Is this ok? Do not use UVLP and OVP functions,P_IN provides a stable 24V,
because Vin range is 0.3v to 24V, but TPS1663 minimum output voltage is 4.5v, so PIN IN&P_IN is supplied independently.
Another question,Our short circuit fault is caused by the short circuit of LED water in rainy days, and the short circuit current in the short circuit is about 20A.
Therefore, the short circuit fault time may be relatively long, and whether the impact short circuit current that occurs repeatedly in the process of automatic retry of blocking will have an impact on the chip
Thanks!