Hi,
I am working on a project,for that i need a little bit clarification i.e.,does IC bq79606A is used for a single cell in a battery?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am working on a project,for that i need a little bit clarification i.e.,does IC bq79606A is used for a single cell in a battery?
Hi Ashok,
Thank you for your question. BQ79606A can be used to monitor down to 3 cells and up to 6 cells. It's main application is automotive battery monitoring:
You can find more details about the features of the device in the BQ79606A-Q1 datasheet ( http://www.ti.com/lit/ds/symlink/bq79606a-q1.pdf )
Best regards,
Leslie
Thanks for your reply,
Can we measure current and temperature along with the voltage?
Hi Ashok,
You may use the GPIOs to take NTC temperature measurements. For current sensing, you would have to get creative with using an INA current sense amplifier device or some other solution as the bq79606A does not have on board current sense.
Best Regards,
Taylor