Hi
My customer is have below questions
By referring to the datasheet, Fig 18 chart is not tally with equation (1)
eg. If Rlimit is 250kohm, the calculated Ilimit 328.6mA while the chart is pointing 450mA . Is it an error or there is another calculation ?
If it is an error, could you share the correct chart.
In section 9.2.2.5 the example, it should depict Figure 17 instead of Figure 18. Was this a typo?
Thanks
Rgds
Kelvin