Please help my client review circuit, circuit such as accessories need to be modified, please help, thank.PAR36-V2.0-Sch-0822.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Please help my client review circuit, circuit such as accessories need to be modified, please help, thank.PAR36-V2.0-Sch-0822.pdf
Hi Hsu,
We have design equations in the data sheet along with Excel spread sheet in the here for the buck boost design that you can use to verify your design:
One comment that I want to make is that this is a 24W design and care must be taken with heat dissipation along with switching frequency and components selection.
Thanks Tuan
The attachment is the design of my reference customer line. Can I help the REVIEW switching frequency and compensator parameters?,Thanks.
Hi Hsu,
If you filled out the requested data on the excel spread sheet correctly then it should work correctly. The switching frequency you filled out is 800Khz so the Rt recommended of 9.3K is correct. The Ris needs to be less than 0.07 Ohm and you have it at 0.08 Ohm. I would use 0.04 to 0.05 Ohm for Ris to reduce power loss on Ris so you can use smaller package there Note that when you change Ris you will change the slope compensation cap along with the compensation component.
As far as compensation, the spread sheet gives you the value if you have filled out everything correctly. However, capacitance value changes with DC bias and the in the spread sheet you have to have the correct effective capacitance along with the dynamic resistance of the LED. We do have an evaluation board that you can obtain and to help with your design if you wish.
Thanks Tuan