Hi,
in one of our products i need to provide 10V and 400mA in OTG mode. The connected battery is a 30Ah 1S Lipo battery.
When connecting the load (a 25 Ohm power resistor) the OTG voltage drops to 3V or Charger disables OTG and the OTG_OCP bit is set. This behavior occurs at a voltage above 8V, below 8V everything works fine. The strange thing is the battery voltage measured by the charger also drops to 3V but measured with an multimeter it is still at 3.8V.
According to the datasheet even 20V and 400mA should not be a problem.
Pleas help.
Regards,
Tom