Hi
Could it be possible to use UPoE devcice as PSE hub?
Should we use Alternative A port?
BestRegards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi na na,
Are you asking if a UPOE switch can interoperate with the TPS23755? If so, the answer is yes. Forced UPOE or LLDP UPOE switch will turn on to 13W.
Note also for UPOE, they will use all four pairs of the cable (both AltA and AltB).
Please let me know if this answers your question. Or please further clarify your question. Thanks!