Other Parts Discussed in Thread: CSD19538Q2, CSD18543Q3A, CSD
We are developing a product use the LM5113 and EPC2035 FET. We just had our first boards assembled and were told by the assembly house that the EPC2035 Bump Die is very difficult to assemble and had to be hand assembled. We have limited space, however we do have enough room to switch to a slightly larger package, such as the SC70, 74, 75, 89 or 96. Can you recommend FET in one of these packages that will work with the LM5113. Our maximum voltage is 18V and the maximum current is about 1.5A.
Thanks,
Bob