This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61178: Switching is audible as load is increased

Part Number: TPS61178

I am using this part to boost the input voltage (6-12V) up to output 12V 4A.  I followed the Webench design tool.  When the AC/DC_12V is at 12V, the circuit works fine with no audible sound.  As the AC/DC_12V input voltage is lowered to less than 8V and/or load increased to around 3A, the circuit starts making audible, squealing sound.  The sound gets louder as the load increases.  I've changed the inductor L1 to 3.3uF, but the sound 190823 - TPS61178 Boost.docxis still there.  Do you have a suggestion?

Thank you,

Vichet