This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR16006: Implement soft-start?

Part Number: LMR16006


I'm using LMR16006. Input is around 19V, output 8.2V, 105mA. There is a divider at the SHDN pin to turn the unit off when input hits 14.5V (100K/8.8K). I'd like to know if there is a way to slow down the turn-on a little bit? The datasheet states that it employs a soft start internally, but is there a manner to simply set up an on-delay as well? Thanks James