IN TESTING THE PFC CONTROLL BOARD I COULDN'T HELP BUT NOTICE THAT THE GDX OUTPUT SIGNALS WERE OSCILLATING BETWEEN 89KhZ TO 115KHz. THE WAY I SEE THIS IS THAT THE GDX SIGNALS COMING FROM THE UCC28070 (Pin #14 & Pin #17) ARE UNSTABLE AND WILL MOST LIKELY DESTROY THE POWER SWITCHES.
NOTE : I AM TESTING ONLY THE SIGNAL PORTION OF THE PFC CONTROL BOARD.
Question #1: IS THIS NORMAL FOR THE UCC28070 IC?
Question #2: IF THIS NOT NORMAL, WHICH IC PINS MIGHT BE CAUSING THE GDX SIGNALS TO SWING BETWEEN 89KhZ TO 115KHz
Question #3 : DO YOU HAVE ANY POSSIBLE SOLUTIONS TO THIS PROBLEM, IF IT IS A PROBLEM?
THANK YOU
EDDIE LOY