The datasheet for the TPS562219A shows two application circuits using a 8.2 nF soft-start capacitor, and figures 26/27 and 39/40 indicate that this value of SS cap should yield a ~1 ms soft-start time. However, when using equation 1 on page 11, a 8.2 nF capacitor gives a calculated value of ~1 us. I suspect that the equation is incorrect, and the time "Tss" is actually calculated in seconds, rather than milliseconds. Can you confirm my thoughts here, or explain otherwise?
Thanks,
-Erik H