Other Parts Discussed in Thread: TPS3820-Q1, TPS3823, TPS3823-Q1, TPS3851, TPS3851-Q1
Hi team,
I am looking for a supervisor chip(AEC-Q100 must) that have Vsense = 3.7V to 4.1V range and standard watchdog function.
Do you have such a device?
So far I could only found TPS3850-Q1 which has adjustable Vsense, but it has window watchdog.
Since I don't want to change the system software already available, window watchdog doesn't match the requirement.
Or is there a way to disable lower boundary of TPS3850-Q1 watchdog function to use it as standard watchdog?
regards,