Dear Specialists,
My customer is encountering the problem when power is up.
I would be grateful if you could advise.
---
About DDR3 termination regulator
The recommended capacitance of the REFOUT output pin is 0.1uF.
Is it possible to change to 10uF?
About the regulator output voltage
The regulator itself has soft-start function, but overshoot has occurred.
I think that the power sequence used for the CPU may not match the recommended sequence for the regulator.
(3.3V = VIN rises after 1.5V = VLDOIN)
But, the CPU sequence cannot be changed.
When a capacitor of about 10uF was connected to REFOUT, overshoot was improved.
For this reason, I would like to confirm that there is no problem.
---
I appreciate your great help in advance.
Best regards,
Shinichi