I AM TESTING WITH NO LOAD AND/OR SWITCHES. I AM TESTING FOR OUTPUT SIGNAL BEFORE GOING FURTHER.
I AM USING A KNOWN WORKING UCC28070 IC THAT I BORROWED FROM A FRIEND WHO ACTUALLY SHOWED ME THAT IT WORKED IN HIS PFC CONTROLLER.
I PUT THAT SAME WORKING IC INTO MY BOARD AND GDA (Pin #14) WAS FLAT-LINE AT 200mV. BUT GDB (Pin #17) WAS WORKING FINE WITH A 10.6V OUTPUT SIGNAL WITH A SLIGHT DUTY CYCLE OSCILLATING BETWEEN 89% TO 96%.
Question 1) WHAT AREA OR PIN # SHOULD I BE CHECKING INTO THAT WOULD CAUSE GDA PIN #14 TO BE FLAT-LINED?
Question 2) EASE PROVIDE EXPLANATION WHY GDA HAS NO OUTPUT SIGNAL AND GDB HAS GOOD OUTPUT SIGNAL?
Question 3) DO YOU HAVE ANY LITERATURE, POST RELATING TO THIS SITUATION?
THANK YOU FOR YOUR SPEEDY RESPONSE.
ED