This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP8860-Q1: FW code

Part Number: LP8860-Q1

Hello

           Customer would like to display 9.35" & 6.75" LCM as below. Which setting needs to modify or any FW code for reference?  Or which EEPROM version suitable to display these LCM. Thank you. 

1. 9.35" LCM: Voltage for LED Backlight: typ. 24.8v, Max. 27.2v, Each serial current Max. 60mA
2. 6.75" LCM: Voltage for LED Backlight: typ. 18.6v, Max. 20.4v, Each serial current Max. 48mA

BR

Patrick