Hi All,
Does anyone explain how to calculate peak current limit (PKLIM)of UC3854? refer to datasheet page 7 "7.5V*2k/10k=1.5V" how 2K and 10K come from?
Thanks
NT
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi All,
Does anyone explain how to calculate peak current limit (PKLIM)of UC3854? refer to datasheet page 7 "7.5V*2k/10k=1.5V" how 2K and 10K come from?
Thanks
NT
The PKLMT comparator for this device is setup with a voltage divider off the reference and attached to the current sense resistor. Please refer to figure 1 the typical application. I do see they used a resistor divider of 10K and 1.6K, which does not match the equation on page 7. In this case the minimum voltage across the current sense resistor that would trip the peak current limit would be (7.5V/10K)*1.6k = 1.2V
Hi Mike,
Can you help us resolve few issues with UC3854. We are developing 5kW power source using UC3854.
We referred to U-134 Application note by TI but was not successful. We have ended up the blowing up the units.
Observations:
Not able to regulate the output voltage