This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

300Vdc input dc-dc converter



Hi,

Can you point me in the right direction?  What ic is best for a high input voltage dc-dc converter with minimal pcb area?  I need to take a 300Vdc input and convert it to 30V (or better yet, 15V).  Is there an ap note/reference design I can refer to? The power range is about 3 Watts.

Thanks,

AJ