This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/TPS54302: TPS54302 - choice of inductor

Part Number: TPS54302

Tool/software: WEBENCH® Design Tools

The choice of inductor for the TPS54302 is confusing.

The evaluation board is set to produce a 5 Volt output from an 8 Volt to 28 Volt input and uses a 10 uH inductor. But if I enter my design requirements (15V input voltage, 0.5 Amp output current), WEBENCH gives me a choice of inductors between about 6 uH and 9 uH and tells me that 10 uH is too large for this design.

So, to cut through the confusion: assuming my requirements (15V input voltage, 0.5 Amp output current), what would be the recommended value for the inductor?