This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23751: PMP21655 output transformer

Part Number: TPS23751

Hello,

PMP21655 is 23V output design. The output transformer is used 7491195112 which datasheet says output voltage is 12V. Is this design able to output 23V with this 12V transformer, 7491195112?

Please let me know why this design can output 23V.

Best regards,

Toshihiro Watanabe

  • Hi Watanabe-san,

    The transformer has 2x 12V windings and so we put them in series to get up to 24V of output voltage (doubles the voltage).

    As an additional note, you can put them in parallel for 12V output and double the current.

    The power stays the same at Type 2 power levels.

    Regards,

    Darwin