This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92074: what't the max power supported, TPS92074

Part Number: TPS92074


Hi Tiers:
i need develop a LED driver,The topology is the APFC+BUCK,

input: AC120-240V, output: 50-240V/ 1A, need support PWM and Analog dimming.

does the TPS92074 can support this project?

if not, which P/N can support this case, thx