This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5569: comparison with LP55231

Part Number: LP5569
Other Parts Discussed in Thread: LP55231,

Hello expert,

Could you kindly help to provide LP5569/LP55231 comparison for us? Thanks a lot!

Best regards,

Ann Lien

  • Hi Ann,

         LP5569 is current sink and LP55231 is high side current source. They are different types of LED driver. I suggest that you may first refer to datasheets for details.

  • Hello Charles,

    Thanks for reply!

    May I know which application will choose LP55231 and LP5569? Since these two devices are all 9-ch solution, I would like to know the difference for it. Thanks a lot!

    Best regards,

    Ann Lien

  • Hi Ann,

        Since the LEDs can be classified into common anode and common cathode, you should choose the device according to the type of LEDs used in your application.

        For common cathode LEDs, the efficiency can be improved because the voltage can be regulated to adapt to different LED forward voltages of different colors. However, structure of common anode LED is helpful to improve the thermal performance.