Other Parts Discussed in Thread: , TPS61202EVM-179, TPS61202, TPS63060, LM2623
Hey everyone - I am looking for a wide input range buck/boost (or boost/buck) that will work from 2V (3V minus 3 diode drops, or roughly 2V, give or take) to 10V. The three diode drops come from an Intrinsic Safety/ATEX requirement. The output is at 5V, current is roughly 300mA into a mostly resistive load. I have tested the EVM for TPS63070 (TPS630702EVM) which is very close to what I need. High end is great and it works well and even will work down to 2V in, but won’t start up at that low a voltage b/c of the positive-going hysteresis – 850mV (yikes!).
I also tested TPS61202 (TPS61202EVM-179) as a boost that can work all the way down below 2V and will start up at approx. 2.1V, that tells me that it’s possible to do. The top end is low, 5.5V, so I can’t use this as a real design choice here.
Do you have any ideas to try that will stretch the startup range of the TPS62070 down to 2V? Can the hysteresis be decreased in any way? The only other solution is a boost (non-synchronous) followed by a buck, but this is really a pretty ugly solution.
Thoughts? thanks - Mark