Other Parts Discussed in Thread: TPS61088, TPS25910, TPS2592AA, LM5176, TPS61178
Hi,
I wanted to ask about the value would be best suited for the inductor and what other changes would be required for this project.
I am looking at replacing the TPS61088 for the TPS55340 (TPS55340PWP). I will be running it of 2S Li-Po batteries, so voltage range will be 6V – 8.4V.
I will also be using the 20V option and have done the calculations for that, so the V3 pin from the CHY100D will also connect to the feedback network (49K9).
Also in place of the TPS2592A, I will be using the TPS25910
So my questions are:
- which is a suitable inductor, value and other information.
- since it does not have an ILIM (TPS55340), would using the ILIM from the TPS25910 be ok? (I’ll be using 66.5 kΩ for 3A limit)
- using the PMEG6045ETPX (60V 6.3A), any issues with this part?
- Setting Output Voltage, I use the following formula as per datasheet: 1.229*(316/20.66+1)= 20.02V
- The 20.66 was derived from: 100k//95k3//127k//49k9.
What else should I take note of? – I am following the schematic from the tidu917.pdf, but using the schematic P1 of the datasheet for the TPS55340 and for Rc and Cc (comp) I will be using the values from p.13 (R3, C4, C5).
Can you please advise what the A values will be for 5V, 9V, 12V & 20V.
Is there anything else I should be made aware of?
Thank you.